Upload the ICVA template
The ICVA extension includes a Project Template that includes a sample Test Plan, a Design Specification, ICVA related custom Work Item types and the Traceability Matrix and Summary Verification Report widgets.
Once the extension is installed, a user with administrative rights to the global Repository can follow the instructions below to install the ICVA project template.
Switch to the Repository level in navigation.
(Click Open Project or Project Group if Repository does not appear in your Recent list.)
Click and select Administration.
Click Project Templates.
Click Upload at the top.
Click Choose File in the Upload project template dialog box.
Navigate to where you installed the ICVA extension and select the ICVAT.zip file.
The path appears beside Select file: in the Upload project template dialog box.
Click Finish.
The ICVA template appears in the Custom Templates section at the bottom of the Project Templates page.
Now when you Create an ICVA project, you will be able to select the IC Verification Assistant template from the Template drop-down menu.