IC Verification Assistant sidebar
You must have a valid Polarion ICVA license to access the IC Verification Assistant sidebar.
The IC Verification Assistant sidebar can be viewed when you have a Document open in Polarion. There you can access and execute most of the operations needed to create and maintain Test Plans.
View the IC Verification Assistant sidebar
Open a Test Plan.
Click on the icon on the top right.
Select IC Verification Assistant sidebar from the drop-down list.
The sidebar appears on the right of your document.
Open the Select Fields dialog box and select the Work Item fields that you’d like visible in the Work Item Properties section of the sidebar. Fields added here are mirrored in the Properties section of the Work Item Properties sidebar. (But here you can also set their visibility.)
Close the sidebar.
Export the current Test Plan revision in Questa’s UCDB format.
Import the results of a merged UCDB file to the current Test Plan and create a new Test Run (Regression results).
Upload a Coverage Model that includes the Coverage Items related to the project.
(Uploaded Coverage Models appear above the buttons.)
Work Item Properties. The fields that you set as visible by clicking then Select Fields.
Add a custom Coverage Item to the Test Plan.
Remove listed: Removes the currently listed Coverage Items from the selected Work Items. They are crossed out in the sidebar until the document is saved. (Or immediately removed if added after the last save.)
Coverage Items that are already added to the Work Item.
Work Item Properties
If you use the ICVA project template then the following fields will be visible:
Weight: Calculate the weighted averages of the parent sections.
0 excludes the item from coverage.
0 for all children excludes the parent scope.
Goal %: The target coverage in % that must be reached.
(Supports fractional values, for example, 99.9%.)
Derived fields
Derived fields update a Verification Requirement with the latest Coverage and Objects from the Regression Results of a Polarion Test Run. They can be used in a Test Plan or other Live Document and are also visible in the IC Verification Assistant sidebar.
Derived field values are updated every time Regression Results are imported. (Their fields remain empty if there is no data from the latest Regression Results.) If you delete the latest Regression Results record, the Derived fields will either be cleared or show the latest Test Run data.
Coverage %: The result of the verification simulation.
Objects: The number of objects that were verified during the verification simulation.
Unimplemented: Whether the verification requirement is implemented or not.
(Can be 1=Implemented or 0=Unimplemented).
Owner: Added as a custom enumeration in Polarion and refers to the responsible user.
Method: Added as a custom enumeration in Polarion and refers to the method used for verification.
ID: The selected item's Work Item ID.