For the first time
When starting the server for the first time, run the Start Apache, PostgreSQL and Polarion Server shortcut.
This shortcut should only be used when the Apache Service, PostgreSQL, and Polarion Server are not running.
Should you choose to run individual startup shortcuts, they should always be run in this sequence:
Click the Start Apache Service shortcut.
Click the Start PostgreSQL Service shortcut.
Click the Start Polarion Server shortcut.
It is normally not necessary to start the Apache or PostgreSQL services again if they are already running. You can check if Apache is running using the Apache Monitor program found in: C:\Polarion\bundled\apache\bin\ApacheMonitor.exe
Use Windows Task Manager to see if the PostgreSQLPolarion service is running.
The first time the Polarion server starts, the following message may appear in a console window.
Not enough data for startup estimation.
This is not an error message. On startup and re-index operations, Polarion estimates and reports the amount of time the operation will take. You see this estimate in the console and log file on subsequent startups, but the first time, no data exists on which to base the estimate.