Manual installation on Linux
It is highly recommended that you run Polarion on one of the supported Linux operating systems and use the automated installation scripts provided in the product distributions for Linux.
There may be cases when Polarion must be installed manually. For example, perhaps an automated installation script doesn’t recognize your system as one of the supported Linux systems due to customization or other factors. Or possibly, your server does not yet have an internet connection, so various packages downloaded during the automated installation are not accessible. Therefore, automated installation cannot proceed. (Scripts inform you if automated installation is not possible).