Link multiple Work Items at once
The technique using the Bulk Edit feature is the same as for single Work Items. The same sections exist in the editor.
Bulk Edit specific features include:
Bulk-edit only modifies selected Work Items.
When you select multiple Work Items, you can create the same link(s) to all the selected Work Items at once.
Direct links can be created because they are storsed in the selected items.
Backlinks, using the Opposite Name, are stored in the backlinked Work Items. So you cannot create backlinks using Bulk Edit.