About reports
Note:
This feature is available in Polarion Requirements, but it is hidden in the default configuration. The topic can be shown in Navigation by changing the Navigation topics configuration. For more information, see Configure Interface Views.
This feature is read-only in Polarion Reviewer.
Scope: Project
The Reports topic provides access to a number of reports related to project source code, and enables you to explicitly launch report calculation.
The Reports topic provides access to the following reports: