Create a new Favorite

In the project where you want to create the new Favorite, navigate to the content you want to access with it. If it is a specific Work Item, you must open the item itself. If you just select it in a Work Item view (Table, for example) the shortcut will lead to the view, not to the item.

  1. In Navigation, click the star icon. The New Shortcut dialog box opens.

  2. (Optional) Change the default Favorite name in the Name field.

  3. Leave the default item Favorite selected in the Type field.

  4. (Optional) Select a different icon from the icon library, and then click Add to create the new Favorite.