Getting Started
Users
| Administrators
| Requirements Engineers
| ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
Developers | Project Managers
| Testing and QA |
This documentation covers all features of Polarion ALM. However, depending on your license, some of the features described may not be available to you.
The following add-on licenses are available:
Polarion Variants: This add-on provides a back-end server component which, when combined with capabilities built into some project templates, adds robust variant management capabilities to the above products.
Polarion IC Verification Assistant: Connects Polarion with Mentor Questa data to capture and trace test records, requirements and results for product validation.
(An ALM license and an additional ICVA license are required.)
Installation documentation
Polarion documentation, including PDF and HTML versions of the installation guides can be found in the Polarion section of SIEMENS' Doc Center.
Extensions
If default functionality doesn't fully meet your needs, you may find a solution on the Polarion ALM Extensions web portal. There you will find a catalog of useful extensions for Polarion ALM solutions ranging from utilities to project templates, to complete features.
The Extensions portal is located at: https://extensions.polarion.com. You can click the Extensions link in the tool view of Navigation to visit the site.