Start and stop Polarion
The Windows installer creates and automatically configures a set of shortcuts that enable you to start and stop the Apache service, start and stop the Polarion server, and launch the web portal in the default browser. There is also a shortcut for the uninstaller program that removes the Polarion installation.
The shortcuts are located in the folder C:\Polarion\polarion shortcuts. The installer places an icon on the desktop that opens this folder in Windows Explorer.
Shortcuts for starting and stopping Apache and the Polarion server