Table of contents
The import feature also imports Table of Contents from the source document. Keep the following points in mind:
Outline numbering is turned on by default, and the TOC of the resulting Document will contain outline numbers in the TOC.
If the source document contains a table of contents, a table of contents will be generated in the resulting Document during import. A manual TOC is replaced by an automatically generated and updated TOC in the Document. Up to five heading levels are recognized and rendered in the TOC of the Document. Properties of the original TOC are saved and used in any subsequent Word Round-trip export.
If the source document contains a TOC, the import preview shows how it will look in the Document after import. The TOC preview is updated when the import preview is updated. TOC items in the import preview are not clickable.
Headings that are recognized as Work Items do not appear in the Document TOC, in both import preview and the LiveDoc Document. If the source document contained a TOC but all headings are recognized as Work Items, then the LiveDoc Document's TOC is initially empty.