Edit an existing Test Run
After creating the new Test Run (or at some other time if something changes before the Test Run is executed), you may want to edit some Test Run properties such as the test environment or Test Run Parameters. After selecting the Test Run you want to edit:
If you are not already on the Test Runs page, click Test Runs in Navigation to access it. Then, in the list of Test Runs, select the Test Run you want to edit. Optionally, use the Visual Query Builder at the top of the page to filter the list of Test Runs. For example, you might query for Manual type tests based on a specific Test Run Template. For more information on the visual query builder tool, see Searching Work Items.
Selecting a Test Run in the table at the top of the page.
If you want to edit the Test Run's properties, click Properties. If any fields of a Test Run are configured as required fields, a red asterisk appears and the field must be filled before you can save the Test Run properties.
If you want to modify the Test Run's page, for example the layout, click (Actions) and select Customize Test Run Page.