Builds
This feature is also available in Polarion Requirements, but it is hidden in the default configuration. The topic can be shown in Navigation by changing the Navigation topics configuration. For more information, see: Configure Interface Views.
This feature is read-only in Polarion Reviewer.
Scope(s): Project
The Builds topic of Navigation enables you to access the current and recent builds of any project. You can find information about the build job(s), create a new build, and access the build results.
The Builds page has two parts. The top half shows a table of recent builds with some basic information about each build listed. It also provides the Create Build for launching a new build, and the Refresh button which refreshes the page with any new builds that may have been launched since you accessed the Builds topic.
The lower half provides information about the build currently selected in the top half of the page. The Build Results section provides access to whatever artifacts the build is configured to generate (often files distribution, installation, etc.) There are also links that provide access to the build log and base directory.
Where to find more information
The Builds topic is an access gateway to the results of builds resulting from Polarion's extensive build-management capabilities.
For information on configuring builds and build management, see:
For more information on working with builds, see: