Project template properties
Project template properties can be specified for custom project templates you create.
If custom templates are used, then to have Polarion replace the Work Item Prefix from template-provided Work Items, add the following lines to your template.properties file:trackerPrefixToReplace=PREFIX, where PREFIX is the Work Item prefix specified in the project template's development project. For example, if your development project's Work Item prefix is "MYTEMPL", then you should specify trackerPrefixToReplace=MYTEMPL in the properties file.
process=.polarion/tracker/fields/workitem-type-enum.xml
These lines are added automatically in templates that ship with Polarion.
For information on project templates and creating custom project templates, see Customizing Project Templates
Each project template may contain a file named template.properties in its root. Use of this file is not required, but is recommended. The file has a standard Java properties file format. The following properties are recognized:
Short template name
Longer template description
Names of parameters required for project creation. Separated by ; (semicolon). The parameter names might contain letters, - (dash), and _ (underscore). Names are case sensitive. The following parameters are predefined:
project-id
project-name
tracker-prefix
trackerPrefixToReplace
List of files/directories to exclude from copying to a new project's directory tree. (template.properties is excluded automatically). Names cannot start with a / (forward slash).
List of text files where the parameters will be substituted during project creation. Files are separated by a ; (semicolon). Names cannot start with a / (forward slash)
Human readable names of parameters defined in the parameters property
template.properties file example
description=Standard software development project for ABC-Corp, Inc. Development Teams
process=.polarion/polarion-project.xml
process=.polarion/tracker/fields/workitem-type-enum.xml
parameters=project-name
param.project-name.name=Project Name
Other files/directories in the template directory are copied to the new project directory during the creation process (except those listed in the skip property). Files listed in the process property are assumed to be text files. During the project creation process, all strings having the form %param-id% are replaced by the actual parameter value. For parameters defined in the parameters property, there is also a predefined parameter project-id, which contains the ID of a newly created project.