Update Subversion
After you update Subversion you must also update Apache (see the next section). Be sure you plan enough time to do both updates.
Visit http://www.apachehaus.com/cgi-bin/download.plx and download
Mod Subversion 1.9.7 for Apache 2.4.x x64.
Unpack the ZIP archive to some temporary folder.
Stop the Polarion and Apache servers.
Stop the existing Svnserve windows service if it is running.
(Ctrl +Alt +Delete → Task Manager → Services tab → Right click on Svnserve and click Stop Service.)
Back up folders $POLARION_HOME$\bundled\apache and $POLARION_HOME$\bundled\svn
Delete the following files:
All files within the $POLARION_HOME$\bundled\svn folder.
(But do not delete the folder itself.)
From folder $POLARION_HOME$\bundled\apache\bin\ …
intl3_svn.dll
libdb48.dll
libsvn_*.dll
From folder $POLARION_HOME$\bundled\apache\modules\ …
mod_authz_svn.so
mod_dav_svn.so
Copy content of the folder within the unpacked temp folder from step two to
$POLARION_HOME$\bundled\svn, so that there is a folder
$POLARION_HOME$\bundled\svn\bin.
Copy the following files in the $POLARION_HOME$\bundled\svn\bin\ … folder...
mod_authz_svn.so
mod_dav_svn.so
…to the $POLARION_HOME$\bundled\apache\modules\ folder.
Copy the following files…
$POLARION_HOME$\bundled\svn\bin\libsvn_*.dll
…to the $POLARION_HOME$\bundled\apache\bin folder.
(Optional). Update Apache.
How do I
Manually Update the bundled third-party softwareUpdate Apache