Plan Work Items
After creating a new Plan and setting its properties, you need to decide which Work Items the team will process and complete during the period of the Plan, and add those Work Items to the Plan. We will refer to this activity as planning Work Items.
The main steps in the process are:
Access the Plan via the Plans topic of Navigation.
Invoke the Open In Table action to open the Plan in the table view, together with the Planning sidebar panel.
Run one or more queries to locate the Work Items to be added to the Plan.
Use control and widgets in the Work Items Table and the Planning Sidebar to plan Work Items by adding them to the Plan.
Prepare to add Work Items
When you have opened a Plan and are ready to plan Work Items into it, you need to open the plan in the Work Items Table view. There, you can run queries to locate the Work Items for the Plan, select them, and add them to the Plan. You can also modify the Plan, removing previously planned items.
You can open a current plan in the table by one of the following:
On the Plan page, click Open in Table.
On the Plan toolbar, click and from the list, select Open in Table.
A new browser tab opens, loading the Table view, creating and running a visual query element to retrieve the Work Items for the Plan, and opening the Planning sidebar panel. You are now ready to begin planning Work Items into the Plan.
Find Work Items for the Plan
If no Work Items have been planned yet, the Table is empty. This is because of the visual query that is specified to retrieve the items in this Plan. You need to remove the query element and build a new query to retrieve all or some of the items you want to add to the Plan. (For information on Work Item queries, see Search Work Items.) You may find it easier to build several simple queries rather than a single complex one. Each query should show some Work Items in the table, and at least some of those should be items you want in the Plan. (If none of them are, you need to revise your query.)
You can use the visual query element Planned In to retrieve the Work Items that have been added (or NOT added) to one specific plan and aggregate the view with items from more than one plan. For more information on using the graphical Query Builder, see Construct Queries Graphically.
Add items to the Plan
Once the table contains items you want to be processed during the Plan period, you can easily add them to the plan:
Select one or more items in the table by checking the box on the respective row(s).
You can add the item to the plan in several ways:
On the Planning sidebar, click Add. A count of items selected for adding appears
Drag a single or multiple selected items from the table to the planning sidebar.
Click the icon on the table row of an item you want to add to the Plan.
When items are added to the Plan, the plan Statistics are updated immediately in the sidebar panel. If you added some items by mistake, or you change your mind after seeing the statistics, you can remove one or more items from the Plan by selecting them in the table and clicking the Remove button.
You can save the changes to the Plan any time during the planning process. Be sure to save changes when you are finished adding items to the plan.
You can review the Work Items in any Plan by selecting the Plan in the Planning sidebar and clicking the (Show Plan Work Items in table) icon.
You can return from the Table to the Plan by clicking on the Plan name in the Planning sidebar.
You can navigate a tree of open Plans, and jump into any listed Plan from the Open Plans section of the Planning sidebar.
When viewing an individual Work Item in the Work Item detail form, the Planned in field lists all Plans that include the item. The field is editable. You can remove a Plan from the field, which removes the item from the removed Plan. You can add another Plan to the field, which adds the current item to the selected Plan.
You can optionally add a column Planned In to the Work Items Table. The column shows all Plans to which a Work Items is added. Clicking on any listed Plan opens the Planning Sidebar and selects the Plan. Because it is multivalued, the table cannot be sorted on this column.
You can also add Work Items to a Plan from the Document Editor. You need to manually open the Planning sidebar and select a Plan. Then click the icon in the Document margin beside any Work Item to add it to the Plan. Note that the type of Work Item must be a type that is allowed in the Plan by its properties. For example, if the Document contains Requirement items, but the Plan properties include only Change Request and Issue type items, you are not be able to add Requirement items to the Plan. You first need to modify the Plan properties to include the Requirement type.