Test step attachments
When manually executing a Test Run, you can optionally add a file attachment to each individual test step, or to a test record. For example, you might attach a screenshot image illustrating the result of a failed test step.
This section describes several important points you need to know about these attachments.
Click Add Attachment to attach a reference file.
Hover over an already attached file and click to remove it.
You can attach a file to a test step or a test record, or remove an attachment from these, while text execution is in progress.
Users can download attachments from Test Steps or the Test Records section of Test Case type Work Items in the Work Item Tracker.
Users can download files attached to a test step result or a test record if the test record is visible on the page of a Test Run.
​Users can download files attached to a test record if the test record is visible in the Test Run Records view.
Attachments are displayed in any Defect items created as a result of failed test steps.
Attachments are not exported to, or imported from Excel during round-trip operations.