Create LiveDoc Document Dialog
Access point: Index page of any Space. Click the icon on the page toolbar, select New LiveDoc Document.
Field | Description |
---|---|
Title | Human readable title of the Document. Supports non-ASCII characters. Contained Work Items can be searched using the Document Title visual query element, entering any part of the value. A value is required. Should not be confused with the Document heading style Title. |
Name (ID) | The unique system identifier of the Document within the project and space. Only ASCII characters may be used. Contained Work Items can be searched using the Document ID visual query element, entering the exact value only. A value is required. |
Type | The Document Type appears only if Document Types are enabled in the system configuration. Field list contains all the Document Types currently configured in the current scope. If present, it is a required field. |
Space (or Subspace) | Name of the Space or Subspace in which the new Document will be stored. Field list contains the names of all spaces and subspaces in the current scope. Value defaults to the space name from which the dialog was invoked. |
Work Item Type | Specifies which type of Work Item the new Document will contain (Addition types can be added after the Document is created.) Field list contains the names of all Work Item types currently configured in the current scope. Value defaults to the type specified as the default type in the Work Item Types configuration in Administration. |
Link Role | Defines the relationship that hierarchically structured Work Items in the Document will have to each other. Field list contains the link roles currently configured in the current scope. |
Enable Outline Numbering | If checked, Work Items in the new Document will automatically be outline numbered based on the Work Item level and position in the Document. |
Prefix | Optional. If specified, the value is prepended to each outline number. |