Client software
Requirement | Description |
---|---|
Operating System | Any operating system that can run the supported web browsers with support for the Flash plugin (see below). If the client user will use a Polarion product supporting data interchange with Microsoft Office®, the client user must run a Windows operating system compatible with a supported version of the Microsoft Office application(s) used. For details, see Appendix: Supported Microsoft Office Versions . |
Web Browser | All you need to use Polarion is a web browser. The most current list of supported browsers and versions is provided in the Release Notes section of the README.html file, delivered in all download distributions of all Polarion products. |
Adobe Flash | The Polarion web portal displays charts and other graphical data about Polarion-managed projects using Adobe Flash. To view these properly using a web browser, the client computer must have Adobe Flash Player installed. You can download it free at http://www.adobe.com/products/flashplayer/. |