Thanks for using or evaluating this Polarion product. This is the README file for version 19.1 of the Polarion ALM product family.
Unless otherwise noted, the information is applicable to:
The navigation menu above leads to information in this file.
Polarion ALM 19.1 is our first service release of 2019 for all Polarion platform-based products.
Visit the Polarion ALM 19.1 – What's New and Noteworthy blog post for details.
IMPORTANT! See the Important Java Information section below for Java changes in 19.1.
This section contains important information about the release including general notes and any known issues you should be aware of.
Updating an existing installation requires a different package than those provided for new installations on the product download pages of the Polarion products web site. Click on the link in the table below to download the update package.
Product | Link |
---|---|
Polarion ALM, QA or REQUIREMENTS | GO TO DOWNLOAD |
NOTE: If you want to update an existing Polarion version prior to version 2012, please seek technical support via the Global Technical Access Center (GTAC).
If you want to try out the latest release as a separate installation before updating your production system, the Update distribution described above will not work for this. Please use the DOWNLOAD button for your operating system on any of these web pages to get an evaluation copy:
If your maintenance subscription is current, you can update from any release after 2015 using the License Key Code you already have. You only need to activate your updated installation, which you can do online or offline. For details, see the bundled HOW_TO_INSTALL_THIS_UPDATE.txt in the update distribution.
If you want to update from version 2014 (including Service Releases) or earlier, you will need to obtain a new license key. You can request it online at https://polarion.plm.automation.siemens.com/getlicense.
If you have questions about, or need help with licensing issues please seek assistance via the Global Technical Access Center (GTAC).
Browser | Version(s) | Notes |
---|---|---|
Google Chrome | Latest | |
Mozilla Firefox | Latest |
Version 67 is recommended for users hoping to tap into the very latest features and improvements.
For organizations or individuals looking for extended support, use Version 60 ESR . |
Microsoft Internet Explorer | 11 | Please be sure to review the following important additional notes. |
Microsoft Edge | Latest |
If running Internet Explorer on Windows Server 2012 (e.g. for testing):
(The above points do not apply when accessing Polarion running on Windows Server 2012 from other clients)
Configuration.txt
file in the update distribution and follow the recommendations regarding Java.In version 2015 SR2, Polarion replaced the integrated H2 database with PostgreSQL in new installations, and continues this with the current release.
In version 2016 and Service Releases, the update package for contains installation scripts that automatically install PostgreSQL to
existing installations and update the system configuration to use PostgreSQL. Before updating a pre-2016 system to this release, please be sure to read the information in the
Configuration.txt
file, bundled in the update distribution.
Several Polarion versions prior to 2014 supported a "Multi-instance" setup on a single or multiple machines. With Polarion 17.x a multi-instance setup is no longer supported on a single machine, but an alternative "Multi-instance" setup on multiple machines is still available . See the "Enterprise Setup Guide" for details. If you still use a pre-2014 "Multi-instance" setup, your administrator should review the section for version 17.0 in the Configuration.txt
file bundled in the update distribution before updating your system.
Polarion no longer supports installation on 32-bit Windows systems. Bundled Apache, Java, Subversion, and PostgreSQL are all 64-bit versions in the installation archives for Windows. A 64-bit OS is now required, and the installer will fail with a message if run on 32-bit Windows. The main potential for impact is on evaluations, for which some people would use 32-bit Windows.
Polarion no longer supports Windows 7 and 8.1 for evaluation installations. Windows 10 is supported.
New Polarion installations on SUSE Linux Enterprise Server (SLES) 11 require that Service Pack 3 be installed, or the installation will fail. Existing installations running on SLES 11 with Service Pack 2 can be updated. However, updating SLES 11 to Service Pack 3 is recommended.
In previous releases, Polarion used the Apache and Subversion binaries from the Apache Haus community for Windows installations. To ensure compliance with internal open source requirements and flexibility in future development, these binaries for Windows are now compiled by Polarion. The binaries compiled by the Apache Haus community are still compatible with Polarion if required by any additional 3rd party customizations.
Relevant system requirements and installation procedures are documented in the Polarion section of SIEMENS PLM Doc Center .
For instructions on how to update an existing Polarion installation, please refer to the HOW_TO_INSTALL_THIS_UPDATE.txt
file
in the root folder of the cumulative update archive after you have downloaded and unpacked it.
Customers who want to use Polarion in a clustered, multi-server environment should download the Polarion Enterprise Setup Guide from in the Polarion section of SIEMENS PLM Doc Center , in addition to the Installation Guide for the relevant operating system(s).
Here are some links to online resources that you may find helpful, especially if you are new to Polarion solutions.
© 2019 Polarion AG