List Favorite Help Topics
To create a list of Favorite help topics:
Locate the help topic you want to make a favorite topic.
Click the Favorites tab, and then click Add.
Note:Click the Favorites tab, select the topic, and then click Display to return to a favorite topic. If you want to rename a topic, select it, type a new name in the Current topic text box and click Add. Select the topic and then click the Remove button to remove a favorite topic.
Related Topics
General TopicsHow to Use the HTML Help Viewer
Browse the Help File
Find a Help Topic in the Table of Contents or in the Index
Find Help Topics Using the Toolbar Buttons (general topics)
Copy a Help Topic
Hide and Show the Navigation Pane
Keyboard Shortcuts in the Help Viewer
Use Context Menu Commands