Produce Parts According to a Percentage Entered into a Data Table
To make the Source produce MUs with a frequency, which you enter into a table:
Select MU selection > Percentage.
Insert a table into a Frame or into a folder in the Class Library.
To designate the type of MU to be produced, do one of the following:
Click . In the dialog Select Object navigate to the folder where the data table is located into which you enter the MUs. Select the name of the Table and click OK.
Drag the table over the text box Table and drop it there.
Enter the name of and the path to the table into the text box next to Table
Enter the names of the MU classes to be produced into the cells below MU into the table.
Enter the percentage portion for each class of MU to be produced into the cells below Portion.
Enter the number of parts to be produced into the cells below Number.
You can, but you do not have to enter a Name or an Attributes table.
Note:When you do not enter a Name, the MUs that the Source produces use the name of their class.
Back to Producing Parts with the Source