Animating the Simulation Model and Viewing the Results
Animating the simulation model and viewing the results provides information about these topics:
Note:
We renamed the following material flow objects in Plant Simulation 14.1:
Up to Version 14.0 | From Version 14.1 on |
---|---|
Assembly | AssemblyStation |
Line | Conveyor |
ParallelProc | ParallelStation |
SingleProc | Station |
Entity | Part |
We renamed the following list objects in Plant Simulation version 14.2.
Up to Version 14.1 | From Version 14.2 on |
---|---|
TableFile | DataTable |
CardFile | DataList |
StackFile | DataStack |
QueueFile | DataQueue |
As we created the models for the Step-by-Step-Help in version 14.0, the screenshots still show the previous names of the list objects.
Compare Modeling in 2D
Compare Modeling in 3D