Installing Product Updates
To install the most recent product update for Plant Simulation, proceed as follows:
Select File > Help > Download Latest Product Updates.
Enter your WebKey Username and your WebKey Password to log on to the GTAC site. You will typically use the WebKey Access Code that the About Tecnomatix Plant Simulation dialog shows.
Download the Plant Simulation software maintenance pack.
Double-click the executable to start the installation.
Note:To run a silent installation, i.e., to install the product update without having to respond to dialogs or messages, open a Command Prompt window and start the downloaded executable with the following command-line parameters: /s /a /s
The maintenance pack uses the registry value HKEY_LOCAL_MACHINE\SOFTWARE\Tecnomatix\eM-Plant\XX.X\eMPlantHome to determine the installation folder. If this registry value does not exist, you can specify the folder with the following command-line parameters:/s /a /s /t "C:\My Plant Simulation Folder"