Tools
Tecnomatix Plant Simulation provides these and a number of other tools:
The Artificial Neural Network for analyzing simulation studies and for forecasting.
The BottleneckAnalyzer and the SankeyDiagram for analyzing and displaying the flow of parts through a plant.
The EnergyAnalyzer for analyzing the energy consumption of machines in your plant.
The ExperimentManager for running experiments with your simulation model. You can also use it for
The GAWizard to optimize models with genetic algorithms.
The Sequential Sampler to start a simulation study, which consists of a single, non-terminating simulation run. It analyzes a single target value.
The Statistics Tools.
The TransferStation for loading, unloading, and reloading parts.
The VariantsGenerator to create frequency tables for attribute variants, which objects of type Source with the setting Attributes >MU selection > Random utilize.
The WorkerChart for showing statistics values of all workers in a single WorkerPool.
We modeled most of the tools as application objects in a Frame. For this reason opening help with F1 and What’s This Help in the dialogs of the objects in the dialogs of the objects do not work. To open help for the tool, select Help > Help on in its dialog.
We modeled the dialogs of the objects with the object Dialog. The dialog windows of the objects do not use the standard Siemens PLM theme, but your Windows theme.
To add any of the tools to the Class Library, click Manage Class Library > Libraries > Tools on the Home ribbon tab.