Conveying direction (described)
The conveying direction of the Part and the Container on the material flow object can be either one of these:
Forward. The part moves with its front in the direction of motion of the material flow.
Lateral right. The part moves with its right hand side in the direction of motion.
Backward. The part is turned by 180° and moves backwards against the direction of motion.
Lateral left. The part moves with its left hand side in the direction of motion.
For illustration purposes we use an icon, which looks like this in its normal state:
We advise against manually changing the conveying direction, but to let the AngularConverter or the Turntable do that.
Changing the conveying direction also permanently affects the attribute ObjectAngle. Changing the attribute ObjectAngle does not change the conveying direction.
SimTalk: