initStat (material flow objects)
Syntax
<Path>.initStat |
The method initStat resets statistics and starts collecting statistics anew. You can use the method initStat if you do not want to include the statistics of the initial stage of the simulation run. You can also reset the statistics at a later time. Plant Simulation will only collect data from that point on.
Note:
When you reset the statistics of an MU class with initStat, this also resets the statistics of the instances.
Example
-- method "resetStatistics" |