origin (general description)
Syntax
<Path>.origin → object |
The method origin accesses the object from which the object designated <Path> was derived most recently.
Compare this example: We copied the object Frame three times and named it Frame1, Frame2, and Frame3. Then, we insert Frame1 into Frame2, and Frame2 into Frame3.
When we call .Frame3.Frame2.Frame1.origin the result will be .Frame2.Frame1, as .Frame2.Frame1 is the object from which .Frame3.Frame2.Frame1 was derived most recently.
Return Value
The return value has the data type object.
Example
if local_change |
Related Topics
Show Origin in the class library
Open Origin in the dialog of the objects
Go to Origin in the dialog of the objects
on the Home Ribbon Tab