Tab Set-Up
On the tab Set-Up you can define how Plant Simulation sets the objects Station, ParallelStation, AssemblyStation, DismantleStation, Drain, and DePortioner up.
Note that you enter the Set-up time on the tab Times.
Compare the sample models: Click the Window ribbon tab, click Start Page > Getting Started > Example Models and click Small Examples. Then, select the respective Category, the Topic, and the Example in the dialog Examples Collection and click Open Model.
Related Topics
The state Setting-Up | |