InputChannels
Syntax
<Path>.InputChannels:table |
The attribute InputChannels designates a table containing the definitions of all input channels
Data Type of the Value You Can Assign
You can assign a value of data type table.
Example
MyChart.InputChannels.delete |
Note:
When you assign a table to the attribute InputChannels with the assignment operator :=, Plant Simulation deactivates inheritance.
Any other kind of writing access, as shown in the example above, does not deactivate inheritance. This means that one of these accesses changes the table the input channels table shares with its origin.
Example
MyChart.Inputchannels := MyDataTable.copy({0,0}..{*,*}) |
Related Topic
Related Topics
Attributes of the ChartAccumulated
Active (Chart)
Category
ChartType
CollectData (Chart)
DataInColumn
DataRange
DataTable (Chart)
DisplayInFrame
Effect
FeedRate
FirstInterval
GapWhenNull
GraphTable
Height (3D charts)
ImageQuality3D
LabelFont
LegendLocation
Mode (Chart)
NullValue
NumIntervals
NumValues
Rotation (Chart)
SampleInterval
Scrollbar
SizeInFrame
StepCurve
StepSize
Subtitle
SubtitleFont
TableFont
Title
TitleFont
UseInputChannels
UseMetricPrefix
XGrid
XGridlines
XLabel
XRange
XScaleMax
XScaleMin
XLog
YGrid
YGridLineInterval
YLabel
YLog
YScaleMax
YScaleMin
ZLabel