Select All (Home ribbon)
The command Select All selects everything.
When you are working with a Frame, the command Select All selects all objects located in the Frame. Instead, you can also press Ctrl+A.
When you are working with a list, the command Select All selects the entire list, i.e., all cells containing an entry.
When you are working with a Method, the command Select All selects the entire source code.