Open Location (Home ribbon)
The command Open Location opens the Frame in which the selected object is located and opens it. It also scrolls the Frame window so that the selected objects will be displayed.
When you are working with a Frame, the command opens the Frame in which this Frame is located.
When you are working with a Method, the command opens the Frame in which the Method is located, or the object for which you defined the user-defined attribute of data type method.
When you are working with a List, the command opens the Frame in which the List is located, or the object for which you defined the user-defined attribute of data type method.
When you are working with icons, the command opens the Frame in which the object is located whose icon you are editing.
Related Topic