Delete Objects (in Frame)
The command Delete Objects deletes the selected object. Be aware that you cannot undo a delete action!
When you are working with a Frame, the command Delete Objects deletes the selected object from the Frame.
When you are working with a List, the command Delete Cells cuts the selected cell or range of cells from the list/table.
Click into the cell at which the range you want to cut starts and drag the mouse to the cell at which the range ends. The list grays the range of cells out and you may then Cut it to the clipboard. Note that Plant Simulation removes the cells you cut from the list and moves the following cells up. Click the row index to select an entire row of cells, click the column header to select an entire column of cells, which you want to cut, i.e., to delete from the list.
When you are working with a Method, the command Delete Text deletes the selected source code.
Plant Simulation opens a dialog in which you can confirm that you want to delete the selected object(s)
Click Yes to delete the object. Hold down the Shift key and click Yes to delete all selected objects.
Click No to not delete the object.
Click Cancel to cancel deleting.
You can deactivate the confirmation query by selecting the check box Confirm under File > Preferences > Modeling > Delete objects.
You can also or press the Del key.
Related Topic