Favorites
In the Favorites window you can add links to the following windows that you need to access frequently:
Frame windows
Method windows
Windows of DataQueue and DataStack
DataList windows
DataTable windows
Windows of user-defined attributes of data type method, table, list, stack, and queue.
To add one of these opened windows to your favorites list, click Add to Favorites .
Note:
To delete the selected favorite from the Favorites list, select it and click the Delete button.
You can then quickly open the respective window by double-clicking its name in the favorites list.