SIMIT
The SIMIT interface provides the interface between Plant Simulation and process control devices, such as PLC controls, via SIMIT, which stands for Simulation & Testing.
The Siemens Website describes SIMIT as:
The simulation platform SIMIT enables comprehensive tests of automation applications and provides a realistic training environment for operator even before the real startup.
To add the SIMIT interface to the Class Library, click Manage Class Library > Basic Objects > InformationFlow on the Home ribbon tab.
Related Topics
Dialog Window of the SIMIT Interface