Setting Parameters in the Model
Tecnomatix Plant Simulation provides a number of ways to enter parameters into your simulation model and to execute simulation runs with these parameters.
You can:
We renamed the following material flow objects in Plant Simulation 14.1:
Up to Version 14.0 | From Version 14.1 on |
---|---|
Assembly | AssemblyStation |
Line | Conveyor |
ParallelProc | ParallelStation |
SingleProc | Station |
Entity | Part |
We renamed the following list objects in Plant Simulation version 14.2.
Up to Version 14.1 | From Version 14.2 on |
---|---|
TableFile | DataTable |
CardFile | DataList |
StackFile | DataStack |
QueueFile | DataQueue |
As we created some of the models for the Online Help in previous versions, some of the screenshots still show the previous names of the objects.
Compare Modeling Random Processes
Compare Executing Simulation Experiments