Objects (LockoutZone)
Syntax
<Path>.Objects:array |
The attribute Objects sets the resource objects, which you want to assign to the LockoutZone designated by <Path>. It also returns these resources.
Data Type of the Value You Can Assign
You can assign a value of data type array which contains the resources.
Example
var a : object[] := [MyStation1, MyStation2] |
print MyLockoutZone.Objects -- might, for example, return |
Related Topic