AdministeredExporters
Syntax
<Path>.AdministeredExporters → array |
The read-only attribute AdministeredExporters returns all Exporters/Workers, which are registered with the Broker designated by <Path>.
The array does not contain all Exporters/Workers that may be reached via the Broker-hierarchy, but only those that are registered directly with the Broker.
Return Value
The return value has the data type array.
Example
print MyBroker.AdministeredExporters |
var t :object[] := MyBroker.AdministeredExporters |
Related Topic
Related Topics
Read-Only Attributes of the BrokerLook up more details
MediatedCapacity (Broker)OpenCapacity
OpenRequests
SatisfiedRequests
StatMediatedCapacity
StatMediationTime
StatMediationTimeDelta
StatMediationTimeMu
StatOpenCapacity
StatOpenRequests
StatSatisfiedRequests
StatStayTime
StatStayTimeDelta
StatStayTimeMu