getRoute (Transporter)
Syntax
<MU-Path>.getRoute → object[] |
The method getRoute returns the route of the Transporter designated by <MU-path> to its destination.
For Transporters, which are not bound to a fixed route network, the method returns the route to the last Marker of this route.
Return Value
The return value is an array of the data type object that contains the objects along the route.
Example
var route := .MUs.Transporter:1.getRoute |
Related Topics
Related Topics
Methods of the Transporterdrive
endFailure (Transporter)
endFailureIn (Transporter)
endPause (Transporter)
endPauseIn (Transporter)
eraseFailureEvents (Transporter)
erasePauseEvents (Transporter)
getLane
getLaneNo
getRouteLength (Transporter)
hitchFront
hitchRear
onLaneA
onLaneB
rotate
setRoute (Transporter)
startFailure (Transporter)
startFailureIn (Transporter)
startPause (Transporter)
startPauseIn (Transporter)
unhitchFront
unhitchRear