HasRouteToDestination (MUs)
Syntax
<MU-Path>.HasRouteToDestination → boolean |
The read-only attribute HasRouteToDestination returns if the Container/Part did find a route to its destination (true) or if it did not find it (false). The method is observable.
Return Value
The return value has the data type boolean.
Example
print .MUs.Part:1.HasRouteToDestination |
Related Topics