StatMaxNumMU
Syntax
<MU-Path>.StatMaxNumMU → integer |
The read-only attribute StatMaxNumMU returns the maximum number of locations the MU class designated by <MU-Path> occupied during the simulation run until the point in time at which you query the statistics. Note that Plant Simulation does not count the maximum number of MUs, but the number of locations occupied simultaneously. Also, loads are not counted.
Return Value
The return value has the data type integer.
Example
print .MUs.Container:1.StatMaxNumMU |
Related Topic
Tab Statistics of the Container
Related Topics
Read-Only Attributes for Accessing Statistics of the Mobile ObjectsHow do I
StatAvgLifeSpan (MUs)StatCount
StatDeleted (MUs)
StatFailTimePortion
StatisticsStartProd
StatMinNumMU (MUs)
StatNumIn (MUs)
StatNumOut (MUs)
StatPauseTimePortion
StatProdFailPortion (MUs)
StatProdFailTime
StatProdPausingPortion (MUs)
StatProdPausingTime
StatProdSetupPortion (MUs)
StatProdSetupTime
StatProdStoppedPortion (MUs)
StatProdStoppedTime
StatProductionTimePortion
StatProdWaitingPortion (MUs)
StatProdWaitingTime
StatProdWorkingPortion (MUs)
StatProdWorkingTime
StatRelativeOccupation (MUs)
StatRelativeOccupationIR (MUs)
StatSetUpTimePortion
StatStoreSetupPortion (MUs)
StatStoreSetupTime
StatStoreStoppedPortion (MUs)
StatStoreStoppedTime
Look up more details
StatStorageTimePortionStatStoreFailPortion (MUs)
StatStoreFailTime
StatStorePausingPortion (MUs)
StatStorePausingTime
StatStoreWaitingPortion (MUs)
StatStoreWaitingTime
StatStoreWorkingPortion (MUs)
StatStoreWorkingTime
StatTranspFailPortion (MUs)
StatTranspFailTime
StatTransportTimePortion
StatTranspPausingPortion (MUs)
StatTranspPausingTime
StatTranspSetupPortion (MUs)
StatTranspSetupTime
StatTranspStoppedPortion (MUs)
StatTranspStoppedTime
StatTranspWaitingPortion (MUs)
StatTranspWaitingTime
StatTranspWorkingPortion (MUs)
StatTranspWorkingTime
StatWaitTimePortion
StatWorkTimePortion