Alpha
Syntax
<Attribute-Path>.Alpha |
The attribute Alpha is a positive number.
Data Type of the Value You Can Assign
You can assign a value of data type real.
You can assign the following attributes/parameters to these distributions:
Distribution | Set of parameters | Range of values for the parameters |
---|---|---|
Alpha, Beta, LowerBound, UpperBound | Alpha > 0, Beta > 0, Upper Bound > Lower Bound | |
Stream, Alpha, Beta, LowerBound, UpperBound | Alpha > 0, Beta > 0, Upper Bound > Lower Bound | |
Stream, Alpha, Theta, LowerBound, UpperBound | Alpha > 0, Theta > 0, Upper Bound > Lower Bound | |
Stream, Alpha, Theta, LowerBound, UpperBound | Alpha > 0, Theta > 0, Upper Bound > Lower Bound | |
Alpha, Beta, LowerBound, UpperBound | Alpha > 0, Beta > 0, Upper Bound > Lower Bound |