Broker Statistics (described)
This topic provides details about the Broker statistics.
The column | Shows the | Read-only attribute |
---|---|---|
Sum Open Requests | total number of open requests. | |
Sum Satisfied Requests | total number of satisfied requests. | |
Sum Open Capacity | total amount of open capacities. | |
Sum Mediated Capacity | total amount of brokered capacities. | |
Mediation Time Sum | sum of the times, which the Broker required to meet all satisfied requests, i. e., the times during which theimporter/importers were waiting for the services. | |
Mediation Time Mean | medium duration of the time the Broker required to meet a single request. | |
Mediation Time Standard Deviation | standard deviation of the medium procurement time. | |
Dwelling Time Sum | sum of the times during which Exporters stayed at importers, i. e., the times during which the services were procured. | |
Dwelling Time Mean | medium duration during which Exporters stayed at a single importer. | |
Dwelling Time Standard Deviation | standard deviation of the dwelling time from the mean value. |
Dwelling Time
This topic provides details about the dwelling time.
When a service is fulfilled by several Workers or Exporters, Plant Simulation records this time interval only once. The same applies for the count. For the time during which the Worker was en-route to his job, statistics counts the time of the Worker who was en-route the longest.
The column | Shows | Read-only attribute |
---|---|---|
Services | the services, which the Broker procures. | |
Count | how often the service in this row was procured, i. e., how often the Exporter/Exporters stayed at the importer/importers. | |
Sum | the sum of the times during which the service in this row was procured. | |
Mean Value | the mean duration of the times during which the service in this row was procured. | |
Standard Deviation | the standard deviation from the mean value of the times during which the service in this row was procured. | |
Minimum | the minimum time during which the service in this row was procured. | |
Maximum | the maximum time during which the service in this row was procured. |
Mediation Time
This topic provides details about the mediation time.
When a service is fulfilled by several Workers or Exporters, Plant Simulation records this time interval only once. The same applies for the count. For the time during which the Worker was en-route to his job, statistics counts the time of the Worker who was en-route the longest.
The column | Shows | Read-only attribute |
---|---|---|
Services | the services, which the Broker procures. | |
Count | how often the importer/importers were waiting for the procurement of the service in this row. | |
Sum | the sum of the times during which the importer/importers were waiting for the procurement of the service in this row. | |
Mean Value | the mean duration of the times during which the importer/importers were waiting for the procurement of the service in this row. | |
Standard Deviation | the standard deviation from the mean value of the times during which the importer/importers were waiting for the procurement of the service in this row. | |
Minimum | the minimum time during which the importer/importers were waiting for the procurement of the service in this row. | |
Maximum | the maximum time during which the importer/importers were waiting for the procurement of the service in this row. |