setCurveSegments
Syntax
<Path>.setCurveSegments(Table:table) |
The method setCurveSegments sets the segments table of the curved object designated by <Path>.
Parameter
The parameter Table of data type table designates the table from which Plant Simulation imports the settings of the segment table.
Note:
The definition of the segments table always shows the original orientation of the segments without a possible rotation or mirroring. The rotation is stored in the attribute ObjectAngle and mirroring is stored in the attribute ObjectMirrored. This allows to keep inheritance of the definition of the segments even when one or more segments are rotated or mirrored.
Example
MyConveyor.setCurveSegments(curveSegmentsTable) |
Related Topics
Import Settings of a Curved Object from Another Simulation Model
Segments table in 3D
_3D.setExtSegments in 3D