startPause (material flow objects)
Syntax
<Path>.startPause |
The method startPause pauses the object designated by <Path>. The method sets the attribute Pause to true.
Parameter
The parameter TimeSpan of data type time designates the time after which, in relation to the simulation time, the object returns to the non-paused state.
The time interval has to be equal to or greater than zero.
Example
@.startPause |
Related Topics
Related Topics
Methods for the State of the Material Flow ObjectsbwBlockList (material flow object)
empty (material flow objects)
endFailure (material flow objects)
endFailureIn (material flow objects)
endPause (material flow objects)
endPauseIn (material flow objects)
endSetupIn
eraseFailureEvents (material flow objects)
erasePauseEvents (material flow objects)
exitBlockList (material flow objects)
exitFree
fwBlockList (material flow objects)
receptive
redraw
setDim
startFailure (material flow objects)
startFailureIn (material flow objects)
startPauseIn (material flow objects)
startProcessing (material flow objects)
unblock