Methods for Accessing Statistics of the Material Flow Objects
The material flow objects provide the methods initStat and statistics for accessing the statistics values they collected which they show on the Tab Statistics.
To view all of the methods and attributes of the material flow object, open the window Show Attributes and Methods. The figure below illustrates the information using the example of the object Source.
Select Show Attributes and Methods on the context menu of the Class Library to show the attributes and methods of the selected Class.
Press the F8 key or click Show Attributes and Methods on the Home ribbon tab of the Frame into which you inserted an instance to show the attributes and methods of the selected Instance.