getAttribute
Syntax
<Path>.getAttribute(AttributeName:string[, byRef Inherited:boolean, byRef CanInherit:boolean]) → any |
The method getAttribute returns the value of an attribute of the object designated by <Path>.
Parameters
The parameter AttributeName of data type string designates the value of the attribute.
When a local variable of data type boolean is passed to the optional parameter Inherited, Plant Simulation assigns true to this variable if the attribute designated by string inherits its value, false if it does not inherit the value.
In case an attribute cannot be inherited, the optional parameter Inherited always returns false.
When a local variable of data type boolean is passed to the optional parameter CanInherit, Plant Simulation assigns true to this variable if the value of the attribute designated by string can be inherited, false if it cannot be inherited.
Return Value
The return value has the data type any.
Example
print MyStation.getAttribute("ProcTime") |
-- checks if inheritance of the attribute 'Accumulating' is active or not |
var inherited:boolean |
var bInherits:boolean |
Related Topics
getAttribute in 3D