deleteAttr
Syntax
<Path>.deleteAttr(AttributeName:string) → boolean |
The method deleteAttr deletes the user-defined attribute of the object designated by <Path>.
Parameter
The parameter AttributeName of data type string designates the user-defined attribute.
Note that you can only delete user-defined attributes for the object for which you created them and for which they are not inherited. Plant Simulation deletes the user-defined attribute from all instances of the object.
Return Value
The return value has the data type boolean.
Example
.MUs.Part.deleteAttr("lotsize") |
@.deleteAttr("Paint") |
Note:
Deleting an object will automatically also delete all of its user-defined attributes.
Related Topics