Stopped (material flow objects)
Syntax
<Path>.Stopped:boolean |
The attribute Stopped sets if the object designated by <Path> is stopped (true) by the LockoutZone or if it is not Stopped (false). Stopped means that all of its processing operations come to a halt.
Note:
When a Worker/Exporter is brokered to the stopped station, it remains brokered to the station while it is stopped. Statistics of the Worker/Exporter does not count this time as waiting.
Data Type of the Value You Can Assign
You can assign a value of data type boolean.
Example
MyStation.Stopped := true |