ObjectMirrored (object icons)
Syntax
<Path>.ObjectMirrored:boolean |
Note:
A 3D Only model does not provide the attribute ObjectMirrored.
The attribute ObjectMirrored sets if the icon of the object designated by <Path> will be mirrored on the y-axis.
Data Type of the Value You Can Assign
You can assign a value of data type boolean.
Example
forkLift.ObjectMirrored := true |
Related Topics
_3D.Rotation for 3D objects