Material Flow Objects
Tecnomatix Plant Simulation provides these objects for simulating the flow of materials through a plant:
Objects for modeling the plant and for controlling the simulation:
The Connector for establishing material flow connections between objects along which the parts move.
The EventController for coordinating and synchronizing the events taking place during a simulation run.
The Frame as the container for creating your simulation models. It might, for example, represent a complex machine, a part of an plant, or the entire plant. The Frame is the principal object facilitating hierarchic modeling.
The Interface for modeling transitions between Frames, i.e., from one part of the model to another. It also facilitates hierarchic modeling.
The material flow objects proper:
The AngularConverter for changing the conveying direction of the mobile objects.
The AssemblyStation for adding mounting parts to a main part, for example doors to a car body.
The Buffer for temporarily holding a large number of parts.
The Converter for conveying a part either straight through or for lifting it onto a laterally moving transport level and then conveying it to the left or right-hand side.
The Conveyor for modeling a conveyor system.
The Cycle for synchronizing the transfer of parts from station to station.
The DismantleStation for removing mounting parts from a main part.
The Drain for removing the parts from the plant after they have been processed. It usually represents the shipping department of your plant.
The FlowControl for modeling strategies for splitting-up and bringing together the flow of materials.
The ParallelStation for modeling stations for processing several parts in parallel at the same time.
The PickAndPlace Robot for picking up a part at one station and placing it onto another station.
The PlaceBuffer for temporarily holding parts in a row, one behind the other.
By default the PlaceBuffer is not part of the built-in objects that the Toolbox provides. You can add it at any time to your simulation model by clicking Manage Class Library on the Home ribbon tab of the Icon Editor.
The Sorter for sorting parts according to different sort criteria.
The Source for producing the parts that move through your model. It usually represents the receiving department of your plant or the main machine producing the parts.
The Station for processing parts on a single processing station. You’ll use it for modeling most of your machines.
The Store for storing parts.
The Track for modeling the track or road on which the Transporter drives.
The Turnplate for modeling a rotating platform, which rotates the loaded parts and ensures the uniform orientation of the leaving parts.
The Turntable for modeling a rotating platform, which moves the part onto one of several connected material flow objects and/or turns it around.
The TwoLaneTrack for modeling a part of a transport line with two lanes on which Transporter traffic moves in opposing directions.
The mobile objects which the material flow objects process or which transport materials:
The Container for modeling pallets, bins, boxes, etc.
The Part for modeling parts being produced and transported.
The Transporter for modeling self-propelled vehicles allowing it to drive on its own on a Track and to transport parts.
The resource objects, which represent the workers and stations related to them:
The Broker for brokering offered services and required services. You might model the supervisor of an plant or the foreman of a shop with it.
The Exporter for providing and exporting services. It represents a group of people, whose individual members you cannot distinguish and whom you cannot address as individuals.
The FootPath for modeling a path on which the worker walks from the workerpool to the workplace.
The ShiftCalendar for modeling the shifts worked in your plant.
The Worker for doing a job on a workplace at a station.
The WorkerPool r for modeling the lounge or the staff room of your plant.
The Workplace for modeling the actual place at the station, where the worker performs his job.
In addition Tecnomatix Plant Simulation provides the TransferStation for loading and unloading stations.
We renamed the following objects in Plant Simulation 14.1 and 14.2:
Up to Version 14.0 | From Version 14.1 on |
---|---|
Assembly | AssemblyStation |
Line | Conveyor |
ParallelProc | ParallelStation |
SingleProc | Station |
Entity | Part |
Up to Version 14.1 | From Version 14.2 on |
---|---|
TableFile | DataTable |
CardFile | DataList |
StackFile | DataStack |
QueueFile | DataQueue |
As we created some of the models for the Online Help in previous versions, some of the screenshots still show the previous names of the objects.
Related Topics